You connect AD v3 to a SmartX server in order to communicate with the SmartX server over a wired (USB) connection. You connect AD v3 to a 24 VDC power supply in order to supply AD v3 with power. You use the Y-shaped cable (SXWADUSBC10002 or SXWADUSBC10003) to connect AD v3 to both the SmartX server and the power supply.
Insert the USB Type-A connector (male) of the Y-shaped cable from AD v3 into the USB host port (female) on the SmartX server.
Insert the 3-pin terminal block (female) of the Y-shaped cable into the intended male connector on the 24 VDC power supply.
The Y-shaped cables are delivered with a 3-pin mating (male) connector.
Wire Color |
Function |
Red |
Positive (+) |
White |
Negative (-) |
Black |
Ground (GND) |
You can now turn on AD v3.