Funkcje: Podstawowa funkcjonalność
Wersja produktu: 3.2, 3.3, 2022
2020-10-15

Showing Abbreviated References

You show abbreviated references to see the last part of the reference.

Pokaż więcej
action_close

References in the List view are abbreviated to save space. An abbreviated reference might only display the first part of the reference but sometimes the last part is the most important one. You can have the system only show the last part of the reference in the list.

For example, if the full reference is ../../IO Resources/Onboard IO/DO 01 and you select to show abbreviated references, the list shows DO 01.

To show abbreviated references
  • In WorkStation, in the List View , click the Show abbreviated references button

     
    action_zoom_plus_stroke
    .

  • Show Abbreviated References
  • List View Toolbar