earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 基本功能
产品版本: 2024, 7.0
2024/12/2

Showing Abbreviated References

You show abbreviated references to see the last part of the reference.

显示更多
action_close

References in the List view are abbreviated to save space. An abbreviated reference might only display the first part of the reference but sometimes the last part is the most important one. You can have the system only show the last part of the reference in the list.

For example, if the full reference is ../../IO Resources/Onboard IO/DO 01 and you select to show abbreviated references, the list shows DO 01.

To show abbreviated references
  • In WorkStation, in the List View , click the Show abbreviated references button

     
    action_zoom_plus_stroke
    .

  • Show Abbreviated References
  • List View Toolbar