earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: RP-C
功能: 硬件
产品版本: 2023, 2024, 7.0
2023/3/30

RP-C Regulatory Compliance and Approvals

This section provides information on regulatory compliance and approvals for the RP-C controllers.

Compliance and approvals for the various RP-C controller models differ depending on whether 24 VAC/VDC or 230 VAC input power is supported and whether wireless connectivity is supported. Most RP-C models are equipped with a wireless chip but some are not.

  • RP-C 24 V models with “-F” in the product name have wireless support:

    RP-C-12A-F-24V, RP-C-12B-F-24V, RP-C-12C-F-24V, and RP-C-16B-F-24V

  • RP-C 24 V models with “-M” in the product name do not have wireless support:

    RP-C-12A-M-24V, RP-C-12B-M-24V, and RP-C-16A-M-24V

  • RP-C 230 V models have wireless support:

    RP-C-16A-F-230V, RP-C-16B-F-230V, and RP-C-16C-F-230V

有关更多信息,请参阅 RP-C Models .

CE - European Union (EU)

RP-C models with wireless support

The RP-C models with wireless support bear the CE mark and comply with the following EU directives:

  • 2014/53/EU Radio Equipment Directive (RED)

  • 2014/35/EU Low Voltage Directive

  • 2011/65/EU Restriction of Hazardous Substances (RoHS) Directive

  • 2015/863/EU amending Annex II to Directive 2011/65/EU

RP-C models without wireless support

The RP-C models without wireless support bear the CE mark and comply with the following EU directives:

  • 2014/30/EU Electromagnetic Compatibility Directive

  • 2014/35/EU Low Voltage Directive

  • 2011/65/EU Restriction of Hazardous Substances (RoHS) Directive

  • 2015/863/EU amending Annex II to Directive 2011/65/EU

UKCA - United Kingdom (UK)

RP-C models with wireless support

The RP-C models with wireless support bear the UKCA mark and complies with the following UK directives:

  • S.I. 2017/1206 - Radio Equipment Regulations 2017

  • S.I. 2016/1101 - Electrical Equipment (Safety) Regulations 2016

  • S.I. 2012/3032 - Restriction of the Use of Certain Hazardous Substances in Electrical and Electronic Equipment Regulations 2012

RP-C models without wireless support

The RP-C models without wireless support bear the UKCA mark and complies with the following UK directives:

  • S.I. 2016/1091 - Electromagnetic Compatibility Regulations 2016

  • S.I. 2016/1101 - Electrical Equipment (Safety) Regulations 2016

  • S.I. 2012/3032 - Restriction of the Use of Certain Hazardous Substances in Electrical and Electronic Equipment Regulations 2012

Federal Communications Commission (FCC)

RP-C 24 V models with wireless support

For the RP-C 24 V models with wireless support (FCC ID: DVE-RPC24), the following statements apply.

This device complies with part 15 of the FCC Rules. Operation is subject to the following two conditions:

  • This device may not cause harmful interference.

  • This device must accept any interference received, including interference that may cause undesired operation.

Changes or modifications not expressly approved by the party responsible for compliance could void the user’s authority to operate this equipment.

This equipment has been tested and found to comply with the limits for a Class B digital device, pursuant to part 15 of the FCC Rules. These limits are designed to provide reasonable protection against harmful interference in a residential installation. This equipment generates, uses and can radiate radio frequency energy and, if not installed and used in accordance with the instructions, may cause harmful interference to radio communications. However, there is no guarantee that interference will not occur in a particular installation. If this equipment does cause harmful interference to radio or television reception, which can be determined by turning the equipment off and on, the user is encouraged to try to correct the interference by one or more of the following measures:

  • Reorient or relocate the receiving antenna.

  • Increase the separation between the equipment and receiver.

  • Connect the equipment into an outlet on a circuit different from that to which the receiver is connected.

  • Consult the dealer or an experienced radio/TV technician for help.

This device, and the antenna used with the device, must be professionally installed. This device may be operated only with the antenna with which it is authorized (see list below). Any antenna that is of the same type and of equal or less directional gain as the antenna that is authorized with the device may be used with the device.

Antenna

Manufacturer

Model (Part number)

Gain

Type

Impedance

Integrated

NA

NA

0.92 dBi

Inverted-F

50 ohm

External

Linx Technologies

ANT-2.4-WRT-MON-SMA

0.8 dBi

Monopole

50 ohm

RP-C 24 V models without wireless support

For the RP-C 24 V models without wireless support, the following statements apply.

This device complies with part 15 of the FCC Rules. Operation is subject to the following two conditions:

  • This device may not cause harmful interference.

  • This device must accept any interference received, including interference that may cause undesired operation.

Changes or modifications not expressly approved by the party responsible for compliance could void the user’s authority to operate this equipment.

This equipment has been tested and found to comply with the limits for a Class B digital device, pursuant to part 15 of the FCC Rules. These limits are designed to provide reasonable protection against harmful interference in a residential installation. This equipment generates, uses and can radiate radio frequency energy and, if not installed and used in accordance with the instructions, may cause harmful interference to radio communications. However, there is no guarantee that interference will not occur in a particular installation. If this equipment does cause harmful interference to radio or television reception, which can be determined by turning the equipment off and on, the user is encouraged to try to correct the interference by one or more of the following measures:

  • Reorient or relocate the receiving antenna.

  • Increase the separation between the equipment and receiver.

  • Connect the equipment into an outlet on a circuit different from that to which the receiver is connected.

  • Consult the dealer or an experienced radio/TV technician for help.

Innovation, Science and Economic Development Canada (ISED)

RP-C 24 V models with wireless support

For the RP-C 24 V models with wireless support (ISED certification number: 24775-RPC24), the following statements apply.

This digital apparatus does not exceed the Class B limits for radio-noise emissions from digital apparatus as set out in the Radio Interference Regulations of the Canadian Department of Communications (ICES-3).

Cet appareil numérique ne dépasse pas les limites de la classe B pour les émissions radio bruit des appareils numériques, tel qu'énoncé dans le Règlement sur le brouillage radioélectrique du ministère des Communications du Canada (NMB-3).

This device contains licence-exempt transmitter(s)/receiver(s) that comply with Innovation, Science and Economic Development Canada’s licence-exempt RSS(s). Operation is subject to the following two conditions:

  • This device may not cause interference.

  • This device must accept any interference, including interference that may cause undesired operation of the device.

L’émetteur/récepteur exempt de licence contenu dans le présent appareil est conforme aux CNR d’Innovation, Sciences et Développement économique Canada applicables aux appareils radio exempts de licence. L’exploitation est autorisée aux deux conditions suivantes:

  • L’appareil ne doit pas produire de brouillage;

  • L’appareil doit accepter tout brouillage radioélectrique subi, même si le brouillage est susceptible d’en compromettre le fonctionnement.

This radio transmitter (24775-RPC24) has been approved by Innovation, Science and Economic Development Canada to operate with the antenna types listed below, with the maximum permissible gain indicated. Antenna types not included in this list that have a gain greater than the maximum gain indicated for any type listed are strictly prohibited for use with this device.

Le présent émetteur radio (24775-RPC24) a été approuvé par Innovation, Sciences et Développement économique Canada pour fonctionner avec les types d'antenne énumérés ci‑dessous et ayant un gain admissible maximal. Les types d'antenne non inclus dans cette liste, et dont le gain est supérieur au gain maximal indiqué pour tout type figurant sur la liste, sont strictement interdits pour l'exploitation de l'émetteur.

Antenna

Manufacturer

Model (Part number)

Gain

Type

Impedance

Integrated

NA

NA

0.92 dBi

Inverted-F

50 ohm

External

Linx Technologies

ANT-2.4-WRT-MON-SMA

0.8 dBi

Monopole

50 ohm

RP-C 24 V models without wireless support

For the RP-C 24 V models without wireless support, the following statements apply.

This digital apparatus does not exceed the Class B limits for radio-noise emissions from digital apparatus as set out in the Radio Interference Regulations of the Canadian Department of Communications (ICES-3).

Cet appareil numérique ne dépasse pas les limites de la classe B pour les émissions radio bruit des appareils numériques, tel qu'énoncé dans le Règlement sur le brouillage radioélectrique du ministère des Communications du Canada (NMB-3).

eu.bac

For the RP-C 230 V controller models RP-C-16A-F-230V and RP-C-16B-F-230V, a eu.bac approved controller application must operate in the controller to maintain compliance with the eu.bac certification. Approved controller applications, which are pre-configured for fan coil, ceiling systems, and other applications, can be downloaded from the Schneider Electric BMS Applications website, bms-applications.schneider-electric.com .

  • Hardware Overview
  • RP-C Controllers
  • RP-C Models
  • RP-C Built-in Power Supply
  • RP Controller Wireless Connectivity