The IP-IO module comes in three models with different I/O point count and different I/O point types.
Model |
I/O Points |
IP-IO-DI10 a |
10 |
IP-IO-UIO10 a |
10 |
IP-IO-UIO5DOFA4 a |
9 |
All IP-IO module models have the same small footprint.
The versatile mix of I/O point types match a wide variety of applications. The universal inputs/outputs are highly flexible and can be configured as either inputs or outputs.
I/O Point Types |
IP-IO-DI10 |
IP-IO-UIO10 |
IP-IO-UIO5DOFA4 |
Digital inputs |
10 |
- |
- |
Universal I/O Type Ub |
- |
10 |
5 |
Relay outputs Form A |
- |
- |
3 |
High power relay outputs Form A |
- |
- |
1 |
The digital inputs can be used for sensing of multiple dry contact digital inputs in applications, such as equipment status monitoring or alarm point monitoring.
Więcej informacji zawiera Digital Inputs .
The universal inputs/outputs are ideal for any mix of temperature, pressure, flow, status points, and similar point types in a building control system.
Więcej informacji zawiera Universal Inputs/Outputs .
The relay outputs support digital Form A point types. The Form A relays are designed for direct load applications.
Więcej informacji zawiera Relay Outputs .
The main application of the high power relay output is to power an electrical heating element directly.
Więcej informacji zawiera High Power Relay Outputs .