earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Produits : IP-IO
Fonctionnalités : Matériel
Version produit : 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
19/07/2021

IP-IO Module Communication Ports

The IP-IO module contains a combination of Ethernet and USB communication ports.

This combination includes the following ports:

  • Two 10/100 Ethernet ports

  • One USB host port

  • One USB device port

When both Ethernet ports are enabled, they function as an onboard Ethernet switch. Disabling the second Ethernet port disables the switching function. The switching function enables flexible network topologies. Pour plus d'informations, voir Advantages to Using External Bindings . The second port also provides a connection point for a laptop running the eCommission SmartX Controllers mobile application.

The two USB ports are reserved for future use.

  • Hardware Overview
  • IP-IO Modules
  • Advantages to Using External Bindings