The IP-IO module is delivered with terminal blocks installed on the device. The IP-IO module uses pluggable terminal blocks, which are easy to install and remove from the device.
The only exception is the high power relay output on the IP-IO-UIO5DOFA4 model, which uses a two-position fixed terminal block due to current requirements.
The wiring recommendations are provided separately. Mer information finns i Wiring .
IP-IO-DI10 has 10 I/O points and the IP-IO module is equipped with four pluggable terminal blocks.
Mer information finns i IP-IO-DI10 Screw Terminals .
IP-IO-UIO10 has 10 I/O points and the IP-IO module is equipped with four pluggable terminal blocks.
Mer information finns i IP-IO-UIO10 Screw Terminals .
IP-IO-UIO5DOFA4 has 9 I/O points and the IP-IO module is equipped with four pluggable terminal blocks and one fixed terminal block.
Mer information finns i IP-IO-UIO5DOFA4 Screw Terminals .