earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Produits : AS-B, Edge Server, Device Administrator, License Administrator, AS-P
Fonctionnalités : Gestion des licences
Version produit : 2024
03/12/2024

Field Server Licensing Overview

Device Administrator is used to manage licenses on field servers.

Software and Features that Require Licenses

A number of software features need licenses.

Pour plus d'informations, voir Software and Features that Require Licenses .

Entitlements, Products, and Licenses

Licenses are bought as products and delivered in Entitlements. An Entitlement is a container that can contain several products. The products contain the licenses and they can differ in quantity and contents.

Field Server Licensing Workflow

Use one of these workflows, depending on if the field servers are connected or not connected to the Internet.

Pour plus d'informations, voir Field Server Licensing on Field Servers Connected to Internet Workflow .

Pour plus d'informations, voir Field Server Licensing on Field Servers not Connected to Internet Workflow .

Certificates

It is recommended to use HTTPS for the communication between Device Administrator and field servers when you manage licenses.

Pour plus d'informations, voir Certificates Managed using Device Administrator .

Return Licenses on Field Servers

You can return licenses from field servers.

Pour plus d'informations, voir Return Licenses on Field Servers .

  • Software and Features that Require Licenses
  • Field Server Licensing on Field Servers Connected to Internet Workflow
  • Inherited Licenses
  • Field Server Licensing on Field Servers Connected to Internet Workflow
  • Field Server Licensing on Field Servers not Connected to Internet Workflow
  • Certificates Managed using Device Administrator
  • Return Licenses on Field Servers