earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos AD v3
Funcionalidades: Hardware
Versión del producto: 3.3, 2022, 2023, 2024
23/07/2021

AD v3 Power Button

AD v3 has a power button that is used to power on the device, to turn off or reboot the device, and to perform other actions.

The power button is located centrally, on the top of the device.

 
action_zoom_plus_stroke Power button
Figura: Power button

The action of the AD v3 power button depends on which mode the device is in and how long the power button is pressed.

Tabla: Power Button Action

Mode

Power Button

Action

Device turned off

Short press

Device starts

Device turned off

Long press (more than 10 seconds)

Recovery (factory reset)

On home screen

Long press (more than 3 seconds)

Dialog box to turn off or reboot device

HMI Kiosk open

Short or long press

Message that the action is blocked

App in Kiosk mode a

Short press (less than 3 seconds)

Prompt to enter password to exit app and return to HMI Kiosk

Any other app open b

Short press

Exit app and return to home screen

Any other app open b

Long press (more than 3 seconds)

Dialog box to turn off or reboot device

Time out (sleep)

Short press (less than 3 seconds)

Wake up

  1. WebStation is typically the app running in Kiosk mode.
  2. Any app not running in Kiosk mode.
  • Hardware Overview
  • Performing a Recovery (Factory Reset) of AD v3
  • AD v3