earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Poradnik

Poradnik


Produkty: WebStation
Funkcje: Alarmy
Wersja produktu: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2018-09-17

Mass Acknowledging Alarms in WebStation

To save time, you can mass acknowledge many alarms in the alarm list at the same time.

Pokaż więcej
action_close

When you acknowledge an alarm, you let other users know that you have seen the alarm. Acknowledging an alarm does not necessarily mean that you are responsible for solving the cause of the alarm.

When you acknowledge an alarm the color of the alarm in the Alarms pane changes. In WebStation the alarm symbol also changes.

An acknowledged alarm does not disappear from the Alarms pane list.

You can acknowledge one alarm or many alarms at the same time.

Uwaga

When you click the Acknowledge button, all alarms that are reset but not acknowledged are automatically selected.

To mass acknowledge alarms in WebStation
  1. In the Alarm list, click the Acknowledge button

     
    action_zoom_plus_stroke
    .

  2. Select the alarms you want to acknowledge.

    • Click the Select all button

       
      action_zoom_plus_stroke
      to select all alarms in the list.

    • Click the Deselect all button

       
      action_zoom_plus_stroke
      to deselect all alarms.

    • Ctrl-click to select each of the alarms you want to acknowledge.

  3. Click OK in the blue acknowledge bar.

  • Alarm Acknowledgements
  • Alarm Toolbar
  • Acknowledging an Alarm in WebStation