Use the Log Pie Properties dialog box to configure and edit a log pie.
Component |
Description |
Add |
Click to add a trend log. |
Display trend log |
Enter the trend log you want to display. |
Calculation method |
Select the calculation method for the trend log. For more information, see Calculation Methods . |
Color |
Select the color for the trend log. |
Period |
Select the period you want to display. |
Caption |
Type a caption for the widget. |
Caption Link |
Select to make a link to an object that is relevant to the values that are displayed in the widget. |
Pie Center |
Select how you want to display the pie center. For more information, see Log Pie . |
Show Legend |
Click True to display the name and color of the trend log in the widget. |
Show Percentage |
Select to display the values in percentage. |
Show Period |
Select to display the period as a legend. |