A point value is used to display the present value of one or many variables as a numerical value.
The colors and calculation method of every log can be changed.
You can configure the color so that different values and value ranges are displayed in different color. You can also add icons in front of the value to make the values easier to read.
For example, you want to create a point value that displays two variables, one called Cooling and one called Heating. The values in cooling between 0 and 10 will be displayed in dark blue and the values from 10 to 15 will be displayed in light blue. The values in Heating between 15 and 20 will be displayed in light red and the values in from 15 to 30 will be displayed in red.
First start by adding the two variables Cooling and Heating.
Edit the variable Cooling. Add two guides in the Guide field and configure them as follows:
Value = 10 and the color dark blue. This makes the color range for all values up to 10 dark blue.
Value = 15 and the color light blue. This makes the color range for all values over 15 light blue.
Edit the variable Heating.
Value = 20 and the color light red. This makes the color range for all values up to 20 light red.
Value = 30 and the color dark red. This makes the color range for all values over 20 dark red.