earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: WebStation
Functionalities: Dashboards
Product version: 2024, 7.0
12/2/2024

Period Chart

A period chart is used to compare trend logs over different time periods.

The trend logs in the chart can be displayed as bar, area, curve, and line. You can change the colors of the trend logs, the calculation method, and the color. You can also change the minimum and maximum value on the Y-axis and the period that is displayed in the chart.

The values of the trend chart can be calculated. For more information, see Calculation Methods .

  • Dashboard Widgets
  • Configuring a Period over Period Chart