Log on to rate and give feedback    1 2 3 4 5 Log on to rate
1
Concept Concept 2/8/2019
Products: (None)
Functionalities: (None)
Product version: 1.0, 1.1, 1.2, 1.3, 1.4, 1.5, 1.6, 1.7, 1.8, 1.9, 2.0, 2.1, 3.0, 3.1

Safety Information

Important Information

Read these instructions carefully and look at the equipment to become familiar with the device before trying to install, operate, service or maintain it. The following special messages may appear throughout this bulletin or on the equipment to warn of potential hazards or to call attention to information that clarifies or simplifies a procedure.

The addition of either symbol to a “Danger” or “Warning” safety label indicates that an electrical hazard exists which will result in personal injury if the instructions are not followed.

This is the safety alert symbol. It is used to alert you to potential personal injury hazards. Obey all safety messages that follow this symbol to avoid possible injury or death.

Danger Danger

DANGER indicates a hazardous situation which, if not avoided, will result in death or serious injury.

Warning Warning

WARNING indicates a hazardous situation which, if not avoided, could result in death or serious injury.

Caution Caution

CAUTION indicates a hazardous situation which, if not avoided, could result in minor or moderate injury.

Notice

NOTICE is used to address practices not related to physical injury.

Please Note

Electrical equipment should be installed, operated, serviced, and maintained only by qualified personnel. No responsibility is assumed by Schneider Electric for any consequences arising out of the use of this material.

A qualified person is one who has skills and knowledge related to the construction, installation, and operation of electrical equipment and has received safety training to recognize and avoid the hazards involved.

Community Content

Product version

Language