earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Концепт

Концепт


Продукты: WebStation
Функции: Dashboards
Версия продукта: 2024, 7.0
02.12.2024

Period over Period Chart

A period chart is used to compare trend logs over different time periods.

The trend logs in the period of period chart can be displayed as bar, area, curve, and line. You can change the colors of the trend logs, the calculation method, and the color. You can also change the minimum and maximum value on the Y-axis and the period that is displayed in the chart.

  • Dashboard Widgets
  • Configuring a Period over Period Chart