Produkty: AS-B, Device Administrator, AS-P
Funkcje: Sprzęt, Zarządzanie licencją
Wersja produktu: 3.2, 3.3, 2022
2022-11-22

Add Entitlement Dialog Box

Use the Add Entitlement dialog box to add an entitlement to Device Administrator.

 
action_zoom_plus_stroke Add Entitlement dialog box
Rysunek: Add Entitlement dialog box

Tabela: Add Entitlement Dialog Box

Component

Description

Entitlement ID

Type the Entitlement ID.

Add Entitlement from file

Click to browse to add an entitlement from a file. The Entitlement file is included in the e-mail that you receive when you made your purchase.

  • Automation Server Licensing Overview