Productos eCommission SmartX Controllers, IP-IO , MP-C, MP-V, RP-C
Funcionalidades: Ingeniería, Dispositivos SmartX IP Controller
Versión del producto: 2022, 2023, 2024, 7.0
10/09/2024
Haga clic para ver la versión actualizada que aún no se ha traducido

Conectarse a un dispositivo mediante Wi-Fi

Se conecta a un dispositivo para empezar las tareas de puesta en marcha.

Mostrar más
action_close

When connecting to a network at the job site, the Commission mobile application device must have either a dynamic or static IP address.

Para obtener más información, consulte Conexión y adquisición de una dirección IP estática .

IP Acquisition Options

Platform

Addressing

Android

DHCP, static

iOS (Apple)

DHCP, static

Windows

DHCP, static, link-local addressing

Aviso

If a network device cannot find a DHCP server, the device performs an autoconfiguration and assigns itself a link-local IP address.

Para obtener más información, consulte Conexión por cable a un solo controlador BACnet/IP .

There are a total of 65,023 usable IP addresses, ranging from 169.254.1.0 to 169.254.254.255.

Para obtener más información, consulte BACnet/IP Controller Commissioning Scenarios .

Network Interface Selection

To use the Commission mobile application on a mobile device that has more than one network interface, you must select the interface you will use. To do this, first determine the IP addresses that are available for your mobile device. You may find the IP address assigned to the selected interface by viewing the device settings. You then select the interface with the correct IP address.

BBMD Implementation

To use the Commission mobile application when you are connected remotely to the controller network, the mobile application can register as a foreign device to a BBMD. To configure the mobile application to register to a BBMD, type the IP address of the BBMD in BBMD address and then select Connect .

When an IP address is present in BBMD address , the mobile application attempts to register with a BBMD at that address. If the BBMD address field is empty, the mobile application connects to the local network.

To connect the Commission mobile application remotely, you must have at least one BBMD on the subnet that you are connecting to. To access the entire remote BACnet internetwork, you must have a networked set of BBMDs. In addition to providing a BBMD, you need to ensure that your mobile device is compatible with the remote network. Typically this requires that you have VPN access to the remote network.

This document is not intended to instruct you how to set up a BBMD for use with the Commission mobile application. For further help with implementing BBMD with the Commission mobile application, consult with the system administrator.

Conectarse a un dispositivo mediante Wi-Fi
  1. En la página Conexión , seleccione Wi-Fi .

  2. En la página Wi-Fi , en el menú desplegable Adaptador , seleccione la dirección IP de su adaptador inalámbrico.

  3. Configure las siguientes funciones opcionales:

    • Dirección de BBMD. Introduzca la dirección IP si se va a conectar a un sitio remoto. Para obtener más información, consulte IP Acquisition and Connectivity .

  4. Pulse en Conectar .

  5. En la página Seleccionar red BACnet , la aplicación móvil Commission seleccionará automáticamente la red local. Si se va a conectar a un sitio remoto, seleccione la casilla junto a la red apropiada. Pulse Descubrir dispositivo .

  6. En la página Lista de dispositivos , seleccione la casilla junto al dispositivo o dispositivos a los que quiera conectarse. Para seleccionar todos los dispositivos que aparecen en la lista, pulse en Seleccionar todos .

    Aviso

    Para filtrar la lista de dispositivos, pulse el icono de Filtro y aplique un filtro. Para obtener más información, consulte Filtrar la lista de dispositivos .

  7. Pulse Siguiente .

Dependiendo de si seleccionó uno o varios dispositivos en el paso 6, podrá acceder a las siguientes páginas:

Cuando llegue a la página Ajustes de dispositivo , se habrá conectado correctamente a un dispositivo único.

Cuando llegue a la página Descargar Firmware , se habrá conectado correctamente a múltiples dispositivos.

  • Conexión del dispositivo
  • Filtrar la lista de dispositivos
  • IP Acquisition and Connectivity