You can filter the device list to help you find a specific device or group of devices more easily.
From the Device List page, select the Filter icon.
Filter the device list by configuring any of the following properties:
Property |
Description |
Show only duplicate devices |
Select the check box to show only duplicate devices in the device list. |
ID Range |
Select and move the maximum and minimum buttons along the scale to adjust the range of devices that appear in the device list. |
Model |
Press Select to choose which SmartX IP models appear in the device list. |
Flow Balance Status |
Press Select to filter the device list based on the flow balance status of either Started , Not started , In progress , or Complete . |
I/O Checkout Status |
Press Select to filter the device list based on the I/O checkout status of either Started , Not started , In progress , or Complete . |
Select Apply .
You can now view the device list based on the filter you have created.