earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Hur göra

Hur göra


Produkter: eCommission SmartX Controllers, IP-IO , MP-C, MP-V, RP-C
Funktionaliteter: Maskinteknik, SmartX IP-kontrollenheter
Produktversion: 3.3, 2022, 2023, 2024, 7.0
2021-07-23

Filtering the Device List

You can filter the device list to help you find a specific device or group of devices more easily.

To filter the device list
  1. From the Device List page, select the Filter icon.

  2. Filter the device list by configuring any of the following properties:

    Property

    Description

    Show only duplicate devices

    Select the check box to show only duplicate devices in the device list.

    ID Range

    Select and move the maximum and minimum buttons along the scale to adjust the range of devices that appear in the device list.

    Model

    Press Select to choose which BACnet/IP device models appear in the device list.

    Flow Balance Status

    Press Select to filter the device list based on the flow balance status of either Started , Not started , In progress , or Complete .

    I/O Checkout Status

    Press Select to filter the device list based on the I/O checkout status of either Started , Not started , In progress , or Complete .

  3. Select Apply .

You can now view the device list based on the filter you have created.

  • Device Connection