earth_america
user_standard Anmelden
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Konzept

Konzept


Produkte: AS-B, Edge Server, Device Administrator, AS-P
Funktionen: Technik, Sicherheit
Produktversion: 2024, 7.0
06.03.2025

SSL Communication Security Settings

The SSL communication security settings can be changed to increase the security of your system. SSL is used for the communication between servers and clients.

You can configure field servers to allow only the SSL communication that you have decided to use.

Hinweis

Loss of data

Configuring the SSL communication to an inaccurate value might block communication.

Failure to follow these instructions can result in loss of data.

  • Certificates and SSL Security in Device Administrator
  • SSL Settings Tab
  • Configuring SSL Communication Security Settings