Produits : AS-B, Edge Server, Device Administrator, AS-P
Fonctionnalités : Matériel, Sécurité
Version produit : 2024, 7.0
03/12/2024

Configuring SSL Communication Security Settings

You configure the SSL communication to increase the security of your system.

Afficher plus
action_close

The SSL communication security settings can be changed to increase the security of your system. SSL is used for the communication between servers and clients.

You can configure field servers to allow only the SSL communication that you have decided to use.

Déclaration

Loss of data

Configuring the SSL communication to an inaccurate value might block communication.

Failure to follow these instructions can result in loss of data.

Déclaration

Loss of data

Configuring the SSL communication to an inaccurate value might block communication.

Failure to follow these instructions can result in loss of data.

To configure SSL communication security settings
  1. In the Device Administrator, click Servers .

  2. In the Server list, click the server.

  3. Click SSL Settings .

  4. In the Blocked SSL Protocol box, add the protocol you want to block.

    Déclaration

    Valid protocol names are tlsv_1, tlsv1_1, tlsv1_2 and tlsv1_3. The tlsv1_2 protocol is valid, but disabling it would prevent you from logging on to WorkStation.

  5. In the Enabled SSL Cipher box, add the cipher you want to enable.

  6. Click Apply .

Déclaration

You can edit SSL configuration in WorkStation Control Panel's Security Settings option or in Device Administrator SSL Security Settings tab.

Pour plus d'informations, voir Security Settings – Control Panel .

Pour plus d'informations, voir SSL Settings Tab .

  • SSL Communication Security Settings
  • Security Settings – Control Panel
  • SSL Settings Tab