earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, Edge Server, Device Administrator, AS-P
Functionalities: Hardware, Security
Product version: 2023, 2024
3/20/2023

Generating an SSL Certificate for an Automation Server Using Device Administrator

You generate an SSL certificate for an automation server so that the server can communicate with Device Administrator using HTTPS.

Show More
action_close

Certificates are used to increase the security of the communication between Device Administrator and automation server.

Certificates are used to establish a trust chain between Device Administrator and the automation servers. A trusted chain communication with HTTPS consists of two parts:

  • An SSL root certificate installed in Windows on the computer that runs Device Administrator

  • An SSL certificate on the automation server

Both Device Administrator and automation servers supports self-signed certificates as well as CA certificates. Device Administrator allows you to create your own self-signed certificate.

Import and export

Certificates can be imported and exported. For example, you have established a trust chain between computer 1, running Device Administrator, and a list of automation servers. You want to access the same automation servers using computer 2. In this case, you install Device Administrator on computer 2, export the SSL root certificate from computer 1, and import it to computer 2.

For more information, see Exporting an SSL Server Root Certificate Using Device Administrator .

For more information, see Importing a Certificate to an Automation Server Using Device Administrator .

Deleting a certificate

Certificates can be deleted from the EBO server using Device Administrator.

For more information, see Deleting an SSL Certificate on an Automation Server Using Device Administrator .

Backup

The certificates are included in the automation server’s backup. You do not need to generate a new certificate if you restore an automation server from a backup generated after the certificate was transferred to the automation server if you retain the original root certificate.

Device Administrator certificate workflow

Use this workflow to create a trusted chain between Device Administrator and automation server using a self-signed certificate.

For more information, see Device Administrator Certificate Workflow .

Use this workflow to create a trusted chain between Device Administrator and automation server using a CA certificate.

For more information, see Device Administrator CA Certificate Workflow .

Certificates and licensing

Certificates generated and installed using Device Administrator must be used when activating licenses.

Certificates generated using Workstation cannot be used for licensing in automation servers since these certificates do not provide a root certificate or other trust chain for validation. If you use WorkStation certificates, we recommend that you generate new ones for your automation servers from Device Administrator when you use licensing in automation servers.

For more information, see Automation Server Licensing Overview .

To generate an SSL certificate for an automation server using Device Administrator
  1. In the Device Administrator, click Servers .

  2. In the Server list, click the automation server name.

  3. Click Server Certificates .

  4. Click Add and then click Generate .

  5. Click OK .

  6. Click OK .

The certificate is now in the automation server list and needs to be transferred to the device to enable communication between the server and Device Administrator.

For more information, see Transferring an SSL Certificate to Automation Server Using Device Administrator .

  • Certificates Managed using Device Administrator
  • Device Administrator Certificate Workflow
  • Transferring an SSL Certificate to Automation Server Using Device Administrator
  • Server Certificates Tab