earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Hur göra

Hur göra


Produkter: AS-B, Edge Server, Device Administrator, AS-P
Funktionaliteter: Maskinteknik, Säkerhet
Produktversion: 2024, 7.0
2025-03-06

Transferring an SSL Certificate to a Field Server Using Device Administrator

You transfer the SSL certificate to the field server to establish a communication using HTTPS between the server and Device Administrator.

Obs!

When you transfer a certificate to a field server, the current active certificate on that field server is deactivated and the new certificate is activated.

Visa mer
action_close

Certificates are used to increase the security of the communication between Device Administrator and field server.

Certificates are used to establish a trust chain between Device Administrator and the automation servers. A trusted chain communication with HTTPS consists of two parts:

  • An SSL root certificate installed in Windows on the computer that runs Device Administrator

  • An SSL certificate on the automation server

Both Device Administrator and automation servers supports self-signed certificates as well as CA certificates. Device Administrator allows you to create your own self-signed certificate.

Import and export

Certificates can be imported and exported. For example, you have established a trust chain between computer 1, running Device Administrator, and a list of field servers. You want to access the samefield servers using computer 2. In this case, you install Device Administrator on computer 2, export the SSL root certificate from computer 1, and import it to computer 2.

Mer information finns i Exporting an SSL Server Root Certificate Using Device Administrator .

Mer information finns i Importing a Certificate to a Field Server Using Device Administrator .

Deleting a certificate

Certificates can be deleted from the EBO server using Device Administrator.

Mer information finns i Deleting an SSL Certificate on a Field Server Using Device Administrator .

Backup

The certificates are included in the field server’s backup. You do not need to generate a new certificate if you restore a field server from a backup generated after the certificate was transferred to the field server if you retain the original root certificate.

Device Administrator certificate workflow

Use this workflow to create a trusted chain between Device Administrator and field server using a self-signed certificate.

Mer information finns i Device Administrator Certificate Workflow .

Use this workflow to create a trusted chain between Device Administrator and field server using a CA certificate.

Mer information finns i Device Administrator CA Certificate Workflow .

Certificates and licensing

Certificates generated and installed using Device Administrator must be used when activating licenses.

Certificates generated using Workstation cannot be used for licensing in field servers since these certificates do not provide a root certificate or other trust chain for validation. If you use WorkStation certificates, we recommend that you generate new ones for your field servers from Device Administrator when you use licensing in field servers.

Mer information finns i Field Server Licensing Overview .

To transfer an SSL certificate to a field server using Device Administrator
  1. In the Device Administrator, click Servers .

  2. In the Server list, click the server name.

  3. Click Server Certificates .

  4. Click Apply .

  5. Click OK .

When the SSL certificate is transferred to the field server, HTTPS communication can be used.

  • Certificates Managed using Device Administrator
  • Device Administrator Certificate Workflow
  • Server Certificates Tab
  • Generating an SSL Certificate for a Field Server Using Device Administrator