earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Пользовательский интерфейс

Пользовательский интерфейс


Продукты: AS-B, Edge Server, Device Administrator, AS-P
Функции: Разработка, Безопасность
Версия продукта: 2024, 7.0
02.12.2024

SSL Root Certificate Dialog Box

Use the SSL Root Certificate dialog box to manage a root certificate.

 
action_zoom_plus_stroke SSL root certificate dialog box
Рисунок: SSL root certificate dialog box

Таблица: SSL Root Certificate Dialog Box

Component

Description

Current root CA certificate

Displays the current root certificate.

Country

Type the country.

State/Province

Type the state/province.

Locality

Type the locality.

Organization

Type the organization.

Unit

Type the unit.

Common name

Type the common name.

Validity period

Enter the calendar end date for the certificate.

Valid days

Type the number of days the certificate is to be valid. The first day is the day when the certificate is generated.

Password

Type a password.

Confirm password

Type the password again.

Export root certificate

Click to export the root certificate.

Install to Windows Certificate Store

Click to install Windows trusted root certificate.

Import certificate

Click to import a self-signed certificate.

Generate root certificate

Click to generate a self-signed certificate.

  • Certificates Managed using Device Administrator