earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Пользовательский интерфейс

Пользовательский интерфейс


Продукты: AS-B, Edge Server, Device Administrator, AS-P
Функции: Разработка, Безопасность
Версия продукта: 2024, 7.0
02.12.2024

Server Certificates Tab

Use the Server Certificate tab to inspect and manage field server certificates.

 
action_zoom_plus_stroke Server Certificates dialog box
Рисунок: Server Certificates dialog box

Таблица: Server Certificate Dialog Box

Component

Description

Name

Displays the name of the certificate.

Description

Displays the description of the certificate.

Issued to

Displays the name of the company that the certificate is issued to.

Issued by

Displays the name of the company that issued the certificate.

Expiration Date

Displays the date the certificate expires.

Active

Displays if the certificate is active.

Add

Click to import or generate a certificate.

Delete

Click to delete the selected certificate.

Set active

Click the selected certificate to make it active.

Export

Click to export the certificate.

Apply

Click to apply all changes made in the Server Certificates tab. This includes transferring certificates to the field servers.

Discard

Click to discard all changes made in the Server Certificates tab.

  • Certificates Managed using Device Administrator