You can increase the security between the Device Administrator and automation servers using certificates and SSL security configuration.
The SSL communication security settings can be changed to increase the security of your system. SSL is used for the communication between servers and clients.
For more information, see SSL Communication Security Settings .
Certificates are used to increase the security of the communication between Device Administrator and automation server.
For more information, see Certificates Managed using Device Administrator .