earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Edge Server, Device Administrator, AS-P
Functionalities: Hardware, Security
Product version: 2024, 7.0
12/3/2024

Certificates and SSL Security in Device Administrator

You can increase the security between the Device Administrator and field servers using certificates and SSL security configuration.

SSL Communication Security Settings in Device Administrator

The SSL communication security settings can be changed to increase the security of your system. SSL is used for the communication between servers and clients.

For more information, see SSL Communication Security Settings .

Certificates in Device Administrator

Certificates are used to increase the security of the communication between Device Administrator and field server.

For more information, see Certificates Managed using Device Administrator .

  • EcoStruxure BMS Server Administration Overview
  • SSL Communication Security Settings
  • Certificates Managed using Device Administrator