Use this workflow to add licenses to automation servers with access to Internet.
Related information can be found in the sections after the flowchart.
Install certificates if you use HTTPS for communication.
Więcej informacji zawiera Device Administrator Certificate Workflow .
Make sure that you have the Entitlements containing the licenses. You need the email with the entitlement during the process.
The Automation servers must have access to Internet for the activation process.
Więcej informacji zawiera Information Technology System Planning Guide .
In Device Administrator, you add entitlements that contains products and licenses.
This is done so that you can view all licenses that are available to be assigned and then activated.
Make sure that you have the HTML entitlement certificate file or the entitlement ID available .
There are two different procedures to add and set up an entitlement when you have an automation server connected to internet:
When the HTML entitlement certificate file is available.
This is the preferred and easiest method.
Więcej informacji zawiera Adding an Entitlement using the HTML file when Automation Server is Connected to License Server (FNO) .
When the HTML entitlement certificate file is not available you must use the entitlement ID.
Więcej informacji zawiera Adding an Entitlement without the HTML file when Automation Server is Connected to License Server (FNO) .
Use the License Products available in the entitlements to assign License Features to the automation servers.
Więcej informacji zawiera Assigning Licenses .
Więcej informacji zawiera Activating Licenses Online .