earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Användargränssnitt

Användargränssnitt


Produkter: AS-B, Edge Server, Device Administrator, License Administrator, License Server, AS-P
Funktionaliteter: Maskinteknik, Licenshantering
Produktversion: 2024, 7.0
2025-03-18

License Settings Dialog Box

The License Settings dialog box is used to view the license settings when troubleshooting. Do not change the settings in this dialog. Changes in this dialog results in license violation. The dialog looks different depending on if it is opened from the Other menu in the   Show Licenses view toolbar, or if it is opened from the Entitlements View .

 
action_zoom_plus_stroke License settings dialog box
Figur: License settings dialog box

Tabell: License Settings Dialog Box

Component

Description

Server address

Displays the address to the server managing the licensing.

User name

Displays user name to the server managing the licensing.

Password

Displays the password to the server managing the licensing.

License model

Displays the license model.

Log level

Select to log the communication between field server and Flex Net Operations administrator server. Enter 1 to start logging.

This is only used when trouble-shooting together with PSS.

  • Field Server Licensing Overview