earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Device Administrator, ​License Administrator, ​License Server, AS-P
功能: 工程, 许可证管理
产品版本: 2024, 7.0
2025/3/18

License Settings Dialog Box

The License Settings dialog box is used to view the license settings when troubleshooting. Do not change the settings in this dialog. Changes in this dialog results in license violation. The dialog looks different depending on if it is opened from the Other menu in the   Show Licenses view toolbar, or if it is opened from the Entitlements View .

 
action_zoom_plus_stroke License settings dialog box
图: License settings dialog box

表格: License Settings Dialog Box

Component

Description

Server address

Displays the address to the server managing the licensing.

User name

Displays user name to the server managing the licensing.

Password

Displays the password to the server managing the licensing.

License model

Displays the license model.

Log level

Select to log the communication between field server and Flex Net Operations administrator server. Enter 1 to start logging.

This is only used when trouble-shooting together with PSS.

  • Centralized Licensing Overview