Use the Entitlements Product Licenses View to view SmartX server licenses.
Component |
Description |
Add entitlement |
Click to add an Entitlement. For more information, see Device Administrator Licenses . |
Add demo license |
Click to add a demo license. For more information, see Device Administrator Licenses . |
Refresh all |
Click to refresh the list. |
Product name |
Displays the product name of the product that contains the licenses in the row for the product. |
Activation ID |
Displays the activation ID. The activation ID is unique for the product and cannot be changed. |
Clients |
Displays the product's number of WebStation clients that can simultaneously connect to the SmartX server. |
SmartDrivers |
Displays the product's number of SmartDrivers that can simultaneously connect to the SmartX server. |
SNMP Notifications |
Displays the product's number of SNMP Notifications that can simultaneously be used on the SmartX server. |
Personal Dashboards |
Displays the product's number of Personalized Dashboards that can simultaneously be used on the SmartX server. |
Total |
Displays the product's total number of licenses. |
Available |
Displays the product's available number of licenses for the product that are not activated. |