earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Device Administrator, AS-P
Functionalities: License Management
Product version: 3.2
3/19/2021

Entitlements Product Licenses View

Use the Entitlements Product Licenses View to view SmartX server licenses.

 
action_zoom_plus_stroke Entitlements Product Licenses view
Figure: Entitlements Product Licenses view

Table: Entitlements Product Licenses View

Component

Description

Add entitlement

Click to add an Entitlement.

For more information, see SmartX Server Licensing Overview .

Add demo license

Click to add a demo license.

For more information, see SmartX Server Licensing Overview .

Refresh all

Click to refresh the list.

Product name

Displays the product name of the product that contains the licenses in the row for the product.

Activation ID

Displays the activation ID. The activation ID is unique for the product and cannot be changed.

SmartDrivers

Displays the product's number of SmartDrivers that can simultaneously connect to the SmartX server.

SNMP Notifications

Displays the product's number of SNMP Notifications that can simultaneously be used on the SmartX server.

Personal Dashboards

Displays the product's number of Personalized Dashboards that can simultaneously be used on the SmartX server.

TimescaleDB

Displays the product's number of TimescaleDB.

MQTT Read/Write

Displays the product's number of MQTT licenses.

Total

Displays the product's total number of licenses.

Available

Displays the product's available number of licenses for the product that are not activated.

  • Entitlements Contents View