earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Пользовательский интерфейс

Пользовательский интерфейс


Продукты: AS-P-3, AS-B, Edge Server, Device Administrator, AS-P
Функции: Управление лицензиями
Версия продукта: 7.0
30.09.2025

Activate Licenses Offline Dialog Box

Use the Activate Licenses Offline dialog box to activate licenses on one or many field servers that are not connected to the Internet.

 
action_zoom_plus_stroke Activate Licenses Offline dialog box
Рисунок: Activate Licenses Offline dialog box

Таблица: Activate Licenses Offline Dialog Box

Component

Description

1. Create request files

Click to create request files with information on the licenses you want to activate.

Более подробную информацию см. EcoStruxure BMS Server Licensing on Servers not Connected to Internet Workflow .

2. Activate request files on License Activation Server (FNO) to receive response files

Click to activate the request files on License Activation Server (FNO) to receive response files.

Более подробную информацию см. EcoStruxure BMS Server Licensing on Servers not Connected to Internet Workflow .

3. Send response files to the selected automation servers

Click to send the response files with the activated licenses to the automation servers to complete the activation process.

Более подробную информацию см. EcoStruxure BMS Server Licensing on Servers not Connected to Internet Workflow .

  • Centralized Licensing Overview
  • EcoStruxure BMS Server Licensing on Servers not Connected to Internet Workflow