earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-L, AS-B, Device Administrator, AS-P
功能: 硬件, 许可证管理
产品版本: 3.0, 3.1
2020/4/17

Assign and Activate Licenses

arrow1_rotationAssign Licenses arrow1_rotationActivate Licenses

When you have added the Entitlement to Device Administrator, you must assign and then activate the licenses on the SmartX servers.

Assign Licenses

Assigning licenses is the process of distribute the licenses from the Entitlement to the SmartX servers in the list.

Activate Licenses

When you have assigned the licenses to the SmartX servers, you must activate the licenses. Activation is required for enabling features that require licenses. Activation is done on the SmartX server level. You can activate licenses for all Smart servers in the list at the same time. Or you can choose to select a subset of servers and activate license for them.

Online activation

Online activation is implemented immediately. Online activation requires that the SmartX server is connect to the internet.

有关更多信息,请参阅 Activating Licenses Online .

Offline activation

Offline activation is used when the SmartX server does not have any access to the internet. Offline activation is a multi-step process.

The offline activation is based on a process where you, after the assigning is completed, create a set of request files using Device Administrator. The request files are then uploaded to the FlexNet Operations Administrator server. Th FlexNet Operations administrator server process the request files and create a set of response files. The response files are downloaded and copied to the computer that runs Device Administrator. From the Device Administrator the response files are sent to the SmartX server. When this is done the licenses are activated.

有关更多信息,请参阅 Offline Activation of Licenses Workflow .

重要:

Activated licenses cannot be deactivated.

  • Device Administrator Licenses
  • Offline Activation of Licenses Workflow
  • Device Administrator Licensing Workflow
  • Activating Licenses Online
  • Assigning Licenses