earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Device Administrator, AS-P
功能: 硬件, 许可证管理
产品版本: 2024
2023/11/30

Activating Request Files to Receive Response Files

You activate request files on License Activation Server (FNO) to receive response files.

显示更多
action_close

Device Administrator is used to manage licenses on field servers.

Software and Features that Require Licenses

A number of software features need licenses.

有关更多信息,请参阅 Software and Features that Require Licenses .

Entitlements, Products, and Licenses

Licenses are bought as products and delivered in Entitlements. An Entitlement is a container that can contain several products. The products contain the licenses and they can differ in quantity and contents.

Field Server Licensing Workflow

Use one of these workflows, depending on if the field servers are connected or not connected to the Internet.

有关更多信息,请参阅 Field Server Licensing on Field Servers Connected to Internet Workflow .

有关更多信息,请参阅 Field Server Licensing on Field Servers not Connected to Internet Workflow .

Certificates

It is recommended to use HTTPS for the communication between Device Administrator and field servers when you manage licenses.

有关更多信息,请参阅 Certificates Managed using Device Administrator .

Return Licenses on Field Servers

You can return licenses from field servers.

有关更多信息,请参阅 Return Licenses on Field Servers .

To activate request files to receive response files
  1. In Device Administrator, click Servers .

  2. Select Show Licenses .

  3. Click Activate .

  4. Click Activate request files on License Activation Server (FNO) to receive response files.

  5. Click OK .

  6. In the Select the zip file containing the request files you want to activate box, select the request file.

  7. Enter the password for the request file.

  8. In the Select the name and location of the zip file that will contain the response file, select a name and a location for the response file.

    The default location and name of the Response file is the same as the Request file.

  9. Click Activate .

  10. Click Close .

  • Field Server Licensing Overview
  • Field Server Licensing on Field Servers not Connected to Internet Workflow
  • Creating the Request Files
  • Sending the Response Files to the Field Server when Activating or Reclaiming Licenses