This section provides recommendations on minimum wire sizes (cross-sectional areas) and maximum wire lengths for the wires connected to the screw terminals of I/O modules, SmartX AS-B servers, and SmartX IP Controller devices. The recommendations are for guidance only. Other wire sizes and lengths may be used, depending on wiring rules and when appropriate.
This section provides recommendations on wire sizes and lengths for the RP-C controller models RP-C-12A, -12B, and -12C.
For more information, see Wire Sizes and Lengths for the RP-C-12A, -12B, and -12C Controllers .
This section provides recommendations on wires sizes and lengths for the RP-C controller model RP-C-16A.
For more information, see Wire Sizes and Lengths for the RP-C-16A Controller .