earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: RP-C, RP-C-EXT-0-10V-4-PD, RP-C-EXT-BL-2-LV-PD, RP-C-EXT-BL-4-HV-PD, RP-C-EXT-DALI-M-PD
功能: 硬件
产品版本: 3.1
2019/12/19

Wire Sizes and Lengths

This section provides recommendations on minimum wire sizes (cross-sectional areas) and maximum wire lengths for the wires connected to the screw terminals of I/O modules, SmartX AS-B servers, and SmartX IP Controller devices. Recommendations on minimum wire size and maximum cable length for the digital inputs of the RP Series expansion modules and the DALI bus of the DALI light modules are also provided. The recommendations are for guidance only. Other wire sizes and lengths may be used, depending on wiring rules and when appropriate.

Wire Sizes and Lengths for the RP-C-12A, -12B, and -12C Controllers

This section provides recommendations on wire sizes and lengths for the RP-C controller models RP-C-12A, -12B, and -12C.

有关更多信息,请参阅 Wire Sizes and Lengths for the RP-C-12A, -12B, and -12C Controllers .

Wire Sizes and Lengths for the RP-C-16A Controller

This section provides recommendations on wires sizes and lengths for the RP-C controller model RP-C-16A.

有关更多信息,请参阅 Wire Sizes and Lengths for the RP-C-16A Controller .

Wire Sizes and Lengths for the Digital Inputs of the RP Series Expansion Modules

This section provides recommendations on wire sizes and lengths for the digital inputs of the RP Series expansion modules.

有关更多信息,请参阅 Wire Sizes and Lengths for the Digital Inputs of the RP Series Expansion Modules .

Wire Sizes and Lengths for the DALI Bus of the RP Series Expansion DALI Light Modules

This section provides recommendations on wire sizes and lengths for the DALI bus of the RP Series expansion DALI light modules.

有关更多信息,请参阅 Wire Sizes and Lengths for the DALI Bus of the RP Series Expansion DALI Light Modules .

  • I/O Wiring
  • Wire Sizes and Lengths for the RP-C-12A, -12B, and -12C Controllers
  • Wire Sizes and Lengths for the RP-C-16A Controller
  • Wire Sizes and Lengths for the Digital Inputs of the RP Series Expansion Modules
  • Wire Sizes and Lengths for the DALI Bus of the RP Series Expansion DALI Light Modules