There is one LED on the RP controller expansion sensor modules. The LED is integrated with the Set button.
Function |
Color |
Status |
Red, Green |
The sensor module Status LED can be configured in the following modes:
Show status mode
Off mode
You configure the Status LED mode in the EcoStruxure Building Operation software. Более подробную информацию см. Configuring RP Controller Expansion Modules .
The sensor module Status LED indicates the condition of the device.
LED Patterns |
Condition |
Recommended action |
Green, constant |
Normal operation, status OK. |
No action required. |
Green constant, with red flash (100 ms every 2 seconds) |
Normal operation, status OK. However, the sensor module has detected and logged an abnormal condition. When the RP-C has retrieved the diagnostics from the sensor module, the Status LED returns to constant green light. Более подробную информацию см. RP Controller Expansion Module Diagnostics . |
No action required. |
Green, flashing (~1 Hz) |
Device is starting or restarting.
|
No action required. |
Green, flashing medium (~2 Hz) |
Device is in maintenance mode. Более подробную информацию см. RP Controller Expansion Module Maintenance Modes . |
To exit the maintenance mode, configure a unique device address in the range supported by the RP-C controller model and then reset the device by disconnecting and reconnecting the device to the RP-C room bus. Более подробную информацию см. Configuring the Room Bus Address for an RP Controller Expansion Sensor Module .Более подробную информацию см. Connecting RP Controller Expansion Modules to an RP Controller . |
Green, flashing fast (~5 Hz) |
Device is initializing. |
No action required. |
Red, flashing (~1 Hz) |
Device is non-operational due to a detected error. Device is forced into maintenance mode. |
Contact Schneider Electric Product Support Services for assistance. |
Red, flashing fast (~5 Hz) |
Device is inoperable due to a detected, non-recoverable error. |
Contact Schneider Electric Product Support Services for assistance or return the device to Schneider Electric. |
Red, constant |
Device is inoperable due to a detected, non-recoverable error. |
Return the device to Schneider Electric. |
The sensor module Status LED is disabled.