earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Explicación de procesos

Explicación de procesos


Productos RP-C, RP-C-EXT-0-10V-4-PD, RP-C-EXT-BL-2-LV-PD, RP-C-EXT-BL-4-HV-PD, RP-C-EXT-DALI-M-PD
Funcionalidades: Hardware
Versión del producto: 3.1, 3.2
19/12/2019

Installing an RP Series Expansion Module on a Flat Surface

You install an RP Series expansion module directly onto a flat surface to properly fasten the device and allow for sufficient ventilation.

Mostrar más
action_close

The RP Series expansion module can be installed on a DIN rail or flat surface.

A DIN rail is a common and convenient technique for installing the RP Series expansion module along with other associated control and monitoring devices. The most efficient ventilation is achieved with the wall-mounted DIN rail oriented horizontally and with adequate space provided between the RP Series expansion module rail and adjacent rails or other devices.

The RP Series expansion module is typically installed horizontally (on a DIN rail going from left to right), with the device label text in the upright position reading left to right.

 
action_zoom_plus_stroke RP Series expansion module installed on a horizontal DIN rail
Figura: RP Series expansion module installed on a horizontal DIN rail

The restrictions on installing the device in other orientations, as well as the normal operating conditions, differ between different types of RP Series expansion modules.

Aviso

EXPANSION MODULE DAMAGE

Follow the installation orientation restrictions that apply to the specific RP Series expansion module.

Failure to follow these instructions can result in equipment damage.

Tabla: Normal Operating Conditions for Different Types of RP Series Expansion Modules

Type of Module

Ambient Temperature

Light modules and high-voltage blind modules

0 to 50 °C (32 to 122 °F)

Low-voltage blind modules

0 to 40 °C (32 to 104 °F)

Under normal operating conditions of 0 to 50 °C (32 to 122 °F), the light modules and high-voltage blind modules can be installed in the following orientations:

  • Horizontally (on a DIN rail going from left to right), with the device label text in the upright position reading left to right. See “a” in the following figure.

  • Vertically (on a DIN rail going from top to bottom), which means that the device is rotated +90 degrees or -90 degrees from the horizontal position. See “b” and “c” in the following figure.

  • Face down from a ceiling. See “d” in the following figure.

  • Rotated 180 degrees from the horizontal position with device label text up and down. See “e” in the following figure.

  • Face up on a horizontal surface. See “f” in the following figure.

 
action_zoom_plus_stroke Installation orientation restrictions for light modules and high-voltage blind modules in normal conditions
Figura: Installation orientation restrictions for light modules and high-voltage blind modules in normal conditions

Under normal operating conditions of 0 to 40 °C (32 to 104 °F), the low-voltage blind modules can be installed in the following orientations:

  • Horizontally (on a DIN rail going from left to right), with the device label text in the upright position reading left to right. See “a” in the following figure.

  • Vertically (on a DIN rail going from top to bottom), which means that the device is rotated +90 degrees or -90 degrees from the horizontal position. See “b” and “c” in the following figure.

  • Face down from a ceiling. See “d” in the following figure.

  • Rotated 180 degrees from the horizontal position with device label text up and down. See “e” in the following figure.

The only installation orientation that is not supported for the low-voltage blind modules is when the device is installed face up on a horizontal surface. See “f” in the following figure. In the face up position, the low-voltage blind module's thermal specifications may be exceeded, which can damage the module.

 
action_zoom_plus_stroke Installation orientation restrictions for low-voltage blind modules in normal conditions
Figura: Installation orientation restrictions for low-voltage blind modules in normal conditions

The RP Series expansion modules can be installed in a standard DIN enclosure.

Aviso

Local panel regulations should be followed when installing the RP Series expansion modules in a distribution panel.

When installing RP Series expansion modules in a DIN enclosure or cabinet, it is recommended to provide ample space between the DIN rails and modules for sufficient ventilation.

 
action_zoom_plus_stroke RP Series expansion modules installed on horizontal DIN rails in a cabinet
Figura: RP Series expansion modules installed on horizontal DIN rails in a cabinet

To help prevent the device from sliding down or sideways on the DIN rail, install an end clip for DIN 35 (part number SXWDINEND10001) tightly against the bottom or rightmost device on the rail. The end clip is easily removed if you bend the snap lock open with a screwdriver.

Aviso

EXPANSION MODULE DAMAGE

Use an end clip (part number SXWDINEND10001) when you install the RP Series expansion module on a vertical DIN rail.

Failure to follow these instructions can result in equipment damage.

 
action_zoom_plus_stroke End clip for DIN 35 fixed across the DIN rail
Figura: End clip for DIN 35 fixed across the DIN rail

All RP Series expansion modules have connectors that allow the matching, external connectors (and cables) for the power supply, outputs, and digitals input to be plugged in on site quickly and easily. Para obtener más información, consulte RP Series Expansion Module Pluggable Connectors .

 
action_zoom_plus_stroke Connectors for outputs (example), power input, and digital inputs
Figura: Connectors for outputs (example), power input, and digital inputs

The RP Series expansion module has four anchor points that can be used to fasten cable ties or other accessories for bundling light weight wires.

 
action_zoom_plus_stroke Anchor points for cable ties
Figura: Anchor points for cable ties

It is recommended to always anchor excess cabling, in accordance with the local regulations, to alleviate all stresses on connectors and cable assemblies. When excess cabling is coiled and left suspended only from the module’s connectors, damage can occur to connectors and/or cable assemblies.

Aviso

CONNECTOR OR CABLE ASSEMBLY DAMAGE

Anchor the excess cabling to alleviate all stresses on connectors and cable assemblies.

Failure to follow these instructions can result in equipment damage.

To install an RP Series expansion module on a flat surface
  1. Refer to the dimensional drawing before installing the RP Series expansion module.

     
    action_zoom_plus_stroke
  2. Ensure that you have the proper mounting hardware and anchoring system.

  3. Check the weight-bearing load before choosing your mounting hardware.

  4. Find a suitable location and surface on which to mount the RP Series expansion module.

  5. Drill three mounting holes that fit number 8 or M4 screws (or anchoring system per manufacturing specification):

    • Two holes for the top two screws on which you hang the RP Series expansion module

    • One hole for the screw at the bottom that helps prevent the device from being lifted off the top two screws

    Use the following drawing to measure out the location of the three holes for the RP Series expansion module.

     
    action_zoom_plus_stroke

    You can also use the 1:1 drill template in the installation sheet that comes with each RP Series expansion module.

  6. Install number 8 or M4 (4 mm) pan head self-tapping screws (with or without anchors) in the two top holes, leaving approximately 5 mm (0.2 inch) space between the head of the screw and the flat surface to accommodate the RP Series expansion module material thickness.

     
    action_zoom_plus_stroke
  7. Fit the two keyhole slots on the back of the RP Series expansion module enclosure to the heads of the mounted screws and then slide the device down in place on the screws.

     
    action_zoom_plus_stroke
  8. Fit the bottom screw (with or without anchor) to the hole at the bottom of the RP Series expansion module and tighten the screw.

     
    action_zoom_plus_stroke
  • RP Series Expansion Module Device Installation
  • Installing an RP Series Expansion Module on a DIN Rail