earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Produits : RP-C, RP-C-EXT-0-10V-4-PD, RP-C-EXT-BL-2-LV-PD, RP-C-EXT-DALI-M-PD
Fonctionnalités : Matériel
Version produit : 3.1
19/12/2019

RP Series Expansion Module Built-in Power Supply

arrow1_rotationDALI Light Modules arrow1_rotation0-10V Light Modules arrow1_rotationLow-voltage Blind Modules

The RP Series expansion light modules with power distribution capability and low-voltage blind modules have a built-in power supply that can accommodate a nominal input voltage of 230 VAC at 50/60 Hz.

The built-in power supply is an integrated AC/DC module, which features a full-wave rectifier, a galvanically isolated DC output, and incorporated electronic components for overvoltage protection, overload protection, and EMI filtering.

With the RP Series expansion module's Power Input galvanically isolated from electronics of the module, the risk of damage due to earth ground currents is reduced.

DALI Light Modules

For the DALI light modules, the built-in power supply is used to convert the AC mains voltage to 18 VDC, which is supplied to the Light outputs for control of the lights.

0-10V Light Modules

For the 0-10V light modules, the built-in power supply is used to convert the AC mains voltage to 10 VDC, which is supplied to the Light outputs for control of the lights.

Low-voltage Blind Modules

For the low-voltage blind modules, the built-in power supply is used to convert the AC mains voltage to 24 VDC, which is supplied to the Blind outputs for control of the blinds.

  • RP Series Expansion Modules and Multi-sensors
  • Light Modules
  • Blind Modules
  • RP-C-EXT-DALI-M-PD
  • RP-C-EXT-0-10V-4-PD
  • RP-C-EXT-BL-2-LV-PD