earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Концепт

Концепт


Продукты: RP-C, RP-C-EXT-0-10V-4, RP-C-EXT-0-10V-4-PD, RP-C-EXT-BL-2-LV-PD, RP-C-EXT-BL-4-HV-PD, RP-C-EXT-BL-SMI-2-LV-PD, RP-C-EXT-BL-SMI-4-HV-PD, RP-C-EXT-DALI, RP-C-EXT-DALI-M-PD, RP-C-EXT-REL-4
Функции: Аппаратное обеспечение
Версия продукта: 2022, 2023, 2024, 7.0
17.12.2021

RP Controller Expansion Module Built-in Power Supply

The RP controller expansion light modules with power distribution capability, low-voltage blind modules, and SMI blind modules have a built-in power supply that can accommodate a nominal input voltage of 230 VAC at 50/60 Hz. Light modules without power distribution capability can accommodate a nominal input voltage of 100 to 277 VAC at 50/60 Hz.

The built-in power supply is an integrated AC/DC module, which features a full-wave rectifier, a galvanically isolated DC output, and incorporated electronic components for overvoltage protection, overload protection, and EMI filtering.

With the RP controller expansion module's Power Input galvanically isolated from electronics of the module, the risk of damage due to earth ground currents is reduced.

DALI Light Modules

For the DALI light modules, the built-in power supply is used to convert the AC mains voltage to 18 VDC, which is supplied to the DALI inputs/outputs for control of the lights.

0-10V Light Modules

For the 0-10V light modules, the built-in power supply is used to convert the AC mains voltage to 10 VDC, which is supplied to the Light outputs for control of the lights.

Low-voltage Blind Modules

For the low-voltage blind modules, the built-in power supply is used to convert the AC mains voltage to 24 VDC, which is supplied to the Blind outputs for control of the blinds.

SMI Low-voltage Blind Modules

For the SMI low-voltage blind modules, the built-in power supply is used to convert the AC mains voltage to 24 VDC, which is supplied to the Blind outputs for powering of the blind motors.

SMI High-voltage Blind Modules

For the SMI high-voltage blind modules, the built-in power supply is used to convert the AC mains voltage to 18 VDC, which is the SMI control voltage.

  • RP Controller Expansion Modules
  • Light Modules
  • Blind Modules
  • RP-C-EXT-DALI-M-PD
  • RP-C-EXT-0-10V-4-PD
  • RP-C-EXT-BL-2-LV-PD
  • RP-C-EXT-DALI
  • RP-C-EXT-0-10V-4
  • RP-C-EXT-BL-SMI-2-LV-PD
  • RP-C-EXT-BL-SMI-4-HV-PD