earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server, AS-B, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 3.1
12/19/2019

Local Backup of EcoStruxure BMS Servers using Device Administrator

You can manually create backup sets using Device Administrator. The backup sets can be saved at any location. One or many EcoStruxure BMS Servers can be backed up at the same time.

To be able to create backup sets of an Enterprise Server or an Enterprise Central, you must run Device Administrator on the same computer as the Enterprise Server or Enterprise Central. You must also run Device Administrator as an administrator. Refer to Windows for information on how to run a program as administrator.

Note:
  • The attached SmartX servers of an Enterprise Server are not included in the backup set of an Enterprise Server.

  • The attached Enterprise Servers are not included in the backup set of an Enterprise Central.

For more information, see Getting Backup set from an EcoStruxure BMS Server using Device Administrator .

  • Manual Backups
  • Getting Backup set from an EcoStruxure BMS Server using Device Administrator