Funkcje: Podstawowa funkcjonalność
Wersja produktu: 3.3, 2022
2021-07-23

Local Backup of EcoStruxure BMS Servers using Device Administrator

You can manually create backup sets using Device Administrator. The backup sets can be saved at any location. One or many EcoStruxure BMS Servers can be backed up at the same time.

To be able to create backup sets of an Enterprise Server or an Enterprise Central, you must run Device Administrator on the same computer as the Enterprise Server or Enterprise Central. You must also run Device Administrator as an administrator. Refer to Windows for information on how to run a program as administrator.

Uwaga
  • The attached automation servers of an Enterprise Server are not included in the backup set of an Enterprise Server.

  • The attached Enterprise Servers are not included in the backup set of an Enterprise Central.

Więcej informacji zawiera Getting Backup set from an EcoStruxure BMS Server using Device Administrator .

  • Manual Backups
  • Getting Backup set from an EcoStruxure BMS Server using Device Administrator