earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Koncept

Koncept


Produkter: CRS-HH-REL-10, RP-C, RP-C-EXT-0-10V-4, RP-C-EXT-0-10V-4-PD, RP-C-EXT-BL-2-LV-PD, RP-C-EXT-BL-4-HV-PD, RP-C-EXT-BL-SMI-2-LV-PD, RP-C-EXT-BL-SMI-4-HV-PD, RP-C-EXT-DALI, RP-C-EXT-DALI-M-PD, RP-C-EXT-REL-4
Funktionaliteter: Maskinvara
Produktversion: 2022, 2023, 2024, 7.0
2022-04-05

RP Controller Expansion Light, Blind, and Relay Modules Regulatory Compliance and Approvals

This section provides information on regulatory compliance and approvals for the RP controller expansion light, blind, and relay modules.

Some of the RP controller expansion modules come in models with or without power distribution capability.

The RP controller expansion modules with power distribution capability include the following models:

  • RP-C-EXT-DALI-M-PD (DALI light module)

  • RP-C-EXT-0-10V-4-PD (0-10V light module)

  • RP-C-EXT-BL-4-HV-PD (High-voltage blind module)

  • RP-C-EXT-BL-2-LV-PD (Low-voltage blind module)

  • RP-C-EXT-BL-SMI-4-HV-PD (SMI high-voltage blind module)

  • RP-C-EXT-BL-SMI-2-LV-PD (SMI low-voltage blind module)

  • RP-C-EXT-REL-4 (4-channel relay module)

The RP controller expansion modules without power distribution capability include the following models:

  • RP-C-EXT-DALI (DALI light module)

  • RP-C-EXT-0-10V-4 (0-10V light module)

  • CRS-HH-REL-10 (10-channel relay module)

CE - European Union (EU)

The RP controller expansion modules bear the CE mark and comply with the following EU directives:

  • 2014/30/EU Electromagnetic Compatibility Directive (EMCD)

  • 2014/35/EU Low Voltage Directive (LVD)

  • 2011/65/EU Restriction of Hazardous Substances (RoHS) Directive

  • 2015/863/EU amending Annex II to Directive 2011/65/EU

UKCA - United Kingdom (UK)

The RP controller expansion modules bear the UKCA mark and complies with the following UK directives:

  • S.I. 2016/1091 - Electromagnetic Compatibility Regulations 2016

  • S.I. 2016/1101 - Electrical Equipment (Safety) Regulations 2016

  • S.I. 2012/3032 - Restriction of the Use of Certain Hazardous Substances in Electrical and Electronic Equipment Regulations 2012

Federal Communications Commission (FCC)

For the RP controller expansion modules, the following statements apply.

This device complies with part 15 of the FCC Rules. Operation is subject to the following two conditions:

  • This device may not cause harmful interference.

  • This device must accept any interference received, including interference that may cause undesired operation.

Changes or modifications not expressly approved by the party responsible for compliance could void the user’s authority to operate this equipment.

This equipment has been tested and found to comply with the limits for a Class B digital device, pursuant to part 15 of the FCC Rules. These limits are designed to provide reasonable protection against harmful interference in a residential installation. This equipment generates, uses and can radiate radio frequency energy and, if not installed and used in accordance with the instructions, may cause harmful interference to radio communications. However, there is no guarantee that interference will not occur in a particular installation. If this equipment does cause harmful interference to radio or television reception, which can be determined by turning the equipment off and on, the user is encouraged to try to correct the interference by one or more of the following measures:

  • Reorient or relocate the receiving antenna.

  • Increase the separation between the equipment and receiver.

  • Connect the equipment into an outlet on a circuit different from that to which the receiver is connected.

  • Consult the dealer or an experienced radio/TV technician for help.

Innovation, Science and Economic Development Canada (ISED)

For the RP controller expansion modules, the following statements apply.

This digital apparatus does not exceed the Class B limits for radio-noise emissions from digital apparatus as set out in the Radio Interference Regulations of the Canadian Department of Communications (ICES-3).

Cet appareil numérique ne dépasse pas les limites de la classe B pour les émissions radio bruit des appareils numériques, tel qu'énoncé dans le Règlement sur le brouillage radioélectrique du ministère des Communications du Canada (NMB-3).

  • RP Controller Expansion Modules
  • Light Modules
  • Blind Modules
  • Relay Modules
  • RP-C-EXT-DALI-M-PD
  • RP-C-EXT-0-10V-4-PD
  • RP-C-EXT-BL-4-HV-PD
  • RP-C-EXT-BL-2-LV-PD
  • RP-C-EXT-DALI
  • RP-C-EXT-0-10V-4
  • RP-C-EXT-BL-SMI-4-HV-PD
  • RP-C-EXT-BL-SMI-2-LV-PD
  • RP-C-EXT-REL-4
  • CRS-HH-REL-10