earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: RP-C, RP-C-EXT-0-10V-4-PD, RP-C-EXT-BL-2-LV-PD, RP-C-EXT-BL-4-HV-PD, RP-C-EXT-DALI-M-PD, RP-C-EXT-MS-BLE
Functionalities: Hardware
Product version: 3.1
12/20/2019

RP Series Expansion Modules and Multi-sensors

arrow1_rotationLight Modules arrow1_rotationBlind Modules arrow1_rotationMulti-sensor

The RP Series expansion modules and multi-sensors provide a range of devices that can be combined to form a connected room solution. The RP Series expansion modules and multi-sensors are connected to the RP-C room bus and provide the RP-C room controllers with I/O expansion and sensors that enable lighting and blind control.

The software application for lighting and blind control runs in the RP-C controller. There is typically one RP-C controller per room. The RP-C controllers are connected to a SmartX server, which controls and manages all the RP-C controllers. There is typically one SmartX server per floor. The SmartX servers are in turn typically connected to an Enterprise Server.

 
action_zoom_plus_stroke RP Series expansion modules and multi-sensors for a connected room solution
Figure: RP Series expansion modules and multi-sensors for a connected room solution

The RP-C controllers can use input data from SmartX Sensors to control the lighting and blinds. The SmartX Sensors are connected to the RP-C sensor bus. The SmartX Sensors provide sensors for temperature, humidity, CO 2 , and occupancy in a room. SmartX Sensor models with touchscreen display enable users to adjust the lighting and blinds in a room. For more information, see SmartX Living Space Sensors Specification Sheet .

In addition, the EcoStruxure Building Engage mobile application allows building occupants to adjust the room comfort settings (room temperature, fan speed, lighting, and window blinds) using a smartphone connected to the RP-C controller through Bluetooth Low Energy. For more information, see Engage .

Light Modules

The RP Series expansion light modules enable control of lights with electrical ballasts and LED drivers.

For more information, see Light Modules .

Blind Modules

The RP Series expansion blind modules enable control of motorized window blinds and shutters.

For more information, see Blind Modules .

Multi-sensor

The RP-C-EXT-MS-BLE multi-sensor connects to the RP-C room controllers and is used for infrared motion detection and luminosity measurements. ​

For more information, see RP-C-EXT-MS-BLE .

  • Hardware Overview
  • Engage
  • Light Modules
  • Blind Modules
  • RP-C-EXT-MS-BLE