The RP Series expansion blind modules enable control of motorized window blinds and shutters.
The blind modules support different types of blind motors.
Module |
Blind Motor |
RP-C-EXT-BL-4-HV-PD |
High-voltage (230 VAC) |
RP-C-EXT-BL-2-LV-PD |
Low-voltage (24 VDC) |
The RP-C-EXT-BL-4-HV-PD blind module connects to the RP-C room controllers and provides I/O expansion for high-voltage blind control.
有关更多信息,请参阅 RP-C-EXT-BL-4-HV-PD .
The RP-C-EXT-BL-2-LV-PD blind module connects to the RP-C room controllers and provides I/O expansion for low-voltage blind control.
有关更多信息,请参阅 RP-C-EXT-BL-2-LV-PD .