You can change regional settings and use different themes to adapt WebStation to your region and your screen.
You can adapt WebStation to your own region regarding units and language.
Mer information finns i Regional Settings .
You can select several themes on how WebStation is presented.
Mer information finns i Theme Settings .
The regional settings and theme settings can be configured on two levels: default system level and user level.
Default system settings are used to make an overall configuration of the system so that all users that have not made any configuration themselves gets the default user setting.
The default system settings might be affected by the lead and shadow mechanism. Mer information finns i Lead and Shadow Relationship .
User setting is used if the user is not satisfied with the default system setting. Users can configure their own regional settings and theme settings that override the default system settings. The user settings are stored on the users account.