You can select several themes themes that control how WebStation is presented.
You can configure WebStation to use dark mode:
Auto: Use the same configuration as in the web browser and operating system. If the web browser and operating system are configured to use dark mode, WebStation will be running in dark mode.
Enable: Enable dark mode regardless of the configuration in the web browser or operating system.
Disable: Disable dark mode regardless of the configuration in the web browser or operating system.
Size mode adjust fonts and icons to the size of your screen:
Auto: Adapts icons and font size to the screen size.
Small: Use small icons and fonts.
Large: Use large icons and fonts.
Accent Color is the color used in the top toolbar in WebStation. This color can be changed.
Accent color can only be configured on default system level.