earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebStation
Functionalities: Basic Functionality
Product version: 2022, 2023, 2024
7/5/2022

Default System Settings – Theme Settings Tab

Use the Theme Settings tab to use dark mode and adjust size on icons and fonts.

 
action_zoom_plus_stroke Default theme settings tab
Figure: Default theme settings tab

Table: Default Theme Settings Tab

Component

Description

Dark Mode

Select if you want to use dark mode. For more information, see Theme Settings .

Size Mode

Select the size of icons and fonts. For more information, see Theme Settings .

Workspace layout

Select the workspace.

Accent Color

Select accent color for the top toolbar. For more information, see Theme Settings .

  • Regional Settings and Theme Settings
  • Theme Settings
  • Lead and Shadow Relationship
  • User Settings – Theme Settings Tab
  • User Settings – Regional Settings Dialog Box
  • Settings – Default Regional Settings Dialog Box