earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Poradnik

Poradnik


Produkty: WebStation
Funkcje: Trendy
Wersja produktu: 3.1, 3.2, 3.3, 2022, 2023
2019-12-19

Adding a Record to a Trend Log List

You manually add trend log records if a log record has been missed and you want to complete the list.

Pokaż więcej
action_close

A trend log list displays all values in the trend log in a list.

In the trend log list, you can perform the following tasks:

  • View all the values and their time stamp.

  • Add and edit records, for example if you knew that some records might be wrong or are missing.

  • Export values as an Excel file.

  • Export values as an xml file.

  • View meter log changes.

  • View events.

  • Change the settings.

 
action_zoom_plus_stroke A Trend log list in WebStation
Rysunek: A Trend log list in WebStation

To add a record to a trend log list
  1. In WebStation, select the trend log list.

  2. On the Trend Log List toolbar, click Add record .

  3. Enter timestamp, value, and comment.

  4. Click Add .

  • Trend Log Lists in WebStation
  • Trend Log List View
  • Trend Log List Toolbar in WebStation
  • Opening a Trend Log List